You are here: Advanced Topics > Motion Techniques > PLCopen Homing > AKD Capture Engine Configuration

AKD Capture Engine Configuration

The AKD capture engine provides a broad range of capabilities for configuration of the capture event(s). Furthermore, it is capable of configuring preconditions to allow the application programmer to specify sequential events or conditions that must be met before the capture event can be triggered. The capture Engine in the AKD is configured with SDO #0x3460 (subindexes 1 to 10). The AKD supports two capture engines (0 and 1); the application programmer must configure the desired engine.

Sub Index # FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances.
1 Trigger for capture engine 0
2 Trigger for capture engine 1
3 Mode for capture engine 0
4 Mode for capture engine 1
5 Capture Event for capture engine 0
6 Capture Event for capture engine 1
7 Precondition edge for capture engine 0
8 Precondition edge for capture engine 1
9 Preselect for capture engine 0
10 Preselect for capture engine 1

The following section details the configuration parameters for the ADK capture engines.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™